Mini-Circuits Mini-Circuits
Shopping Cart Home Page Link Shopping Cart    My Account
     

Content on this page requires a newer version of Adobe Flash Player.

Get Adobe Flash player


 

 

 

 

 

 

"To travel hopefully is a better thing than to arrive, and the true success is to labor."
-Robert Louis Stevenson
Find Your Product
Browse Our
Product Line

Model Number Search
Advanced Model Search
yoni logo
Searching millions of actual data points to meet your specific requirements
Latest News & Events
Other News and Events, Click Here

MCL  April 5, 2013 Partnership Promises Free RF/MW Models!
Teaming with Modelithics, precision EDA simulation models for Mini-Circuits new YAT/RCAT series fixed DC to 18 GHz attenuators are available for free download.

MCL April 5, 2013 Mini-Circuits' Attenuators Achieve Industry Recognition
DC to 18 GHz, surface-mount YAT series fixed attenuators take center stage in this Microwaves & RF magazine cover story. "Tiny Attenuators Set Levels To 18 GHz".

MCL March 5, 2013 Mini-Circuits introduced an additional 22 High Pass Filters to its already broad product line of coaxial high pass filters. With sixteen (16) ZX75HP and six (6) ZFHP filters, the Mini-Circuits line of low cost, off-the-shelf,  super small filters are ideal for applications from test labs to quick-fix filter solutions in any RF system.

MCL  March 5, 2013 Mini-Circuits is expanding our ever growing coaxial adapter line with the introduction of new flange-mounted models up to 18 GHz and by adding our first 3.5mm format adapters which operate up to 34 GHz.  Extending the current product line in both feature and frequency.

MCL  March 5, 2013 Mini-Circuits enhances its already comprehensive line of broadband high power directional couplers by introducing and upgrading our existing product line to now include bi-directional couplers covering frequencies from 380 to 9000 MHz Our new ZGBDC series of bi-directional couplers provide an outstanding combination of high power and low loss and directivity performance.  Models up to 3.6 GHz meet the IP67 standard for rugged outdoor applications. This series uses suspended substrate and airline technology for industry-leading low-loss performance and are available with 6, 10 and 20 coupling ratio.

MCL  March 4, 2013 Mini-Circuits updates our already extensive line of YAT ultra-small (2x2mm) surface mount fixed attenuators with an additional eight values up to 30 dB! Offered in 1dB increments up to 10 dB and then additional five values up to 30dB, the YAT series of attenuators are ideally suited for a wide array of system application to equalize gains and losses throughput a distributed RF chain while consuming minimum board footprint and parts placements.

MCL  March 4, 2013 Mini-Circuits releases the new TMC2-43X+, a new version of our popular TCM Series transforming 2:1 impedance ratios over the impressive range of 10 to 4000 MHz Used in 50 ohm, 75ohm or other impedance systems, the TCM2-43X+ offers outstanding amplitude and phase balance over the entire band. This tiny transformer is an outstanding candidate for a wide range of differential circuits such as ADC, DAC, differential mixers, QAM Mod/demod or when used in harmonic suppression circuits such as broadband push pull amplifier architectures.

MCL  March 4, 2013 Mini-Circuits added two new models to our existing SYVA series Voltage Variable Attenuator product line. The SYVA-16+ and SYVA-30+ cover frequencies from 10 to 30 MHz and bring to these bands the same insensitivity to source and load impedance, flat frequency performance and high dynamic range as all other SYVA series VVA’s .

MCL  March 1, 2013 The Mini-Circuits website was recently updated to include a policy on Conflict Minerals! The Dodd-Frank Wall Street Reform and Consumer Protection Act of 2010 requires publicly traded companies to confirm that Tin, Gold, Tungsten and Tantalum are not sourced from the Democratic Republic of the Congo and neighboring countries. Although Mini-Circuits is privately held, we recognize the need to promote the humanitarian intent of this legislation and support our customers in their efforts to comply. In addition to clearly stating our policy, Mini-Circuits will also provide EICC format responses to assist customers in their data collection.

MCL  January 21, 2013 New Wideband Amplifier Delivers Incredibly Flat Gain, High IP3 and Excellent Return Loss at Low DC Power Levels! Mini-Circuits new GVA-60+ amplifier features a frequency range from 10 MHz to 5 GHz, optimized to deliver incredibly flat gain (20 ±0.3 dB), high IP3 (29-40 dBm), and an input return loss of 17-20 dB with no external matching for VHF/UHF/IF applications and more!

MCL  December 21, 2012 New 75 Ω Amplifiers “Right on the Money” for CATV, FTTx, MoCA, and Satellite Systems Mini-Circuits new PGA-106 series of amplifiers deliver a winning combination of high dynamic range, low noise, and flat gain, fine-tuned to meet specific customer demands across a wide range of 75 Ω systems!

MCL  November 14, 2012 Hurricane Sandy Update! - Important information and Message from Mini-Circuits President. Thank you for your patience and we appreciate all the support we have received from customers and suppliers. We are pleased to announce that we are well on track with our recovery and are now better than 94% back to full operational capacity...

MCL  November 4, 2012 Hurricane Sandy Update! - Important information and Message from Mini-Circuits President. As we near the end of the first week after hurricane Sandy devastated the mid-Atlantic region and particularly the greater New York area, we are pleased to announce that all of our members in the New York region are safe and unharmed; and the spirit of Mini-Circuits is alive and well as evidenced in our 90% operational status

MCL  October 26, 2012 New Ultra Wideband Coaxial Doubler, SMD Transformer, and Flat Gain/High Dynamic Range Coaxial Amplifier! Mini-Circuits keeps pushing its industry-leading lineup of wideband RF, IF, and microwave products even wider, to deliver higher levels of performance for both new and old applications, and meed the "big picture" requirements of the engineers who design and bulid them! For example...

MCL  October 16, 2012 N-Type/Quick Lock SMA Cables Speed DUT Connect/ Disconnect Cycles for Network Analyzers! Mini-Circuits has released 4 new Quick Lock SMA Cable Assemblies that also include a male N-type connector—ideal for use with 50Ω N-type network analyzers!

MCL  October 11, 2012 Eight New High-Linearity Frequency Mixers Now Available at Mini-Circuits! Mini-Circuits continues to add to its industry-leading mixer lineup, releasing 8 new HJK and LAVI designs with third-order intercepts as high as 33 dBm, and L-R isolation up to 55 dB! Frequency ranges vary from 235 MHz to 4.5 GHz...

MCL October 3 2012 Precise Tilt Compensation Easier than Ever, with SMD Voltage-Variable Equalizer from Mini-Circuits! Our new VAEQ-1000-75+ equalizer makes it easy to flatten the frequency response of individual CATV runs and other 75Ω circuitry—from 50 MHz all the way up to 1GHz!

MCL  September 24, 2012 New Ceramic Hermetic Limiters, Amplifiers, and High Gain Mixers Deliver Ultra-Rel Performance in Ultra-Low-Profile Cases! Mini-Circuits exclusive ceramic hermetic technology is ideal anywhere long-term reliability adds bottom-line value. For more proof, just take a look at our new CLM Limiters, CMA Amplifiers, and MRA High-Gain Mixers!

MCL  September 13, 2012 New Surface-Mount Limiter Protects Against Undesired High-Power Signals from 200 kHz up to 3 GHz! Mini-Circuits new RLM-33-2W+ limiter protects LNAs and other sensitive circuitry from spikes and power surges (+12 to +33 dBm), with minimal small-signal losses (0.25 dB typ) across an incredible 13+-octave bandwidth!

MCL  September 05, 2012 New Ultra Wideband Amplifier Delivers Super-Flat Gain from 100 MHz to 18 GHz! Mini-Circuits new ZVA-183W+ amplifier is catching the eye of ultra wideband application designers everywhere, with its high, flat gain (27 ± 2dB typical) across an incredibly wide, 7+-octave frequency range!...