Build Log
  

Build started: Project: ZtModular, Configuration: Debug|Win32

Command Lines
  
Creating temporary file "d:\soft\Project Examples\MCL_ZT_Modular_Examples\mcl_io.dll_Examples\VC++ (MFC)\ZtModular\ZtModular\Debug\RSP00001033402288.rsp" with contents
[
/Od /D "WIN32" /D "_WINDOWS" /D "_DEBUG" /D "_AFXDLL" /D "_UNICODE" /D "UNICODE" /Gm /EHsc /RTC1 /MDd /Yu"stdafx.h" /Fp"Debug\ZtModular.pch" /Fo"Debug\\" /Fd"Debug\vc80.pdb" /W3 /c /Wp64 /ZI /TP ".\ZtModularDlg.cpp"
]
Creating command line "cl.exe @"d:\soft\Project Examples\MCL_ZT_Modular_Examples\mcl_io.dll_Examples\VC++ (MFC)\ZtModular\ZtModular\Debug\RSP00001033402288.rsp" /nologo /errorReport:prompt"
Creating temporary file "d:\soft\Project Examples\MCL_ZT_Modular_Examples\mcl_io.dll_Examples\VC++ (MFC)\ZtModular\ZtModular\Debug\RSP00001133402288.rsp" with contents
[
/OUT:"D:\soft\Project Examples\MCL_ZT_Modular_Examples\mcl_io.dll_Examples\VC++ (MFC)\ZtModular\Debug\ZtModular.exe" /INCREMENTAL /MANIFEST /MANIFESTFILE:"Debug\ZtModular.exe.intermediate.manifest" /DEBUG /PDB:"d:\soft\Project Examples\MCL_ZT_Modular_Examples\mcl_io.dll_Examples\VC++ (MFC)\ZtModular\debug\ZtModular.pdb" /SUBSYSTEM:WINDOWS /ENTRY:"wWinMainCRTStartup" /MACHINE:X86 ".\Debug\stdafx.obj"

".\Debug\ZtModular.obj"

".\Debug\ZtModularDlg.obj"

".\Debug\ZtModular.res"

".\Debug\ZtModular.exe.embed.manifest.res"
]
Creating command line "link.exe @"d:\soft\Project Examples\MCL_ZT_Modular_Examples\mcl_io.dll_Examples\VC++ (MFC)\ZtModular\ZtModular\Debug\RSP00001133402288.rsp" /NOLOGO /ERRORREPORT:PROMPT"
Creating temporary file "d:\soft\Project Examples\MCL_ZT_Modular_Examples\mcl_io.dll_Examples\VC++ (MFC)\ZtModular\ZtModular\Debug\RSP00001233402288.rsp" with contents
[
/out:".\Debug\ZtModular.exe.embed.manifest" /notify_update /manifest

".\Debug\ZtModular.exe.intermediate.manifest"
]
Creating command line "mt.exe @"d:\soft\Project Examples\MCL_ZT_Modular_Examples\mcl_io.dll_Examples\VC++ (MFC)\ZtModular\ZtModular\Debug\RSP00001233402288.rsp" /nologo"
Creating temporary file "d:\soft\Project Examples\MCL_ZT_Modular_Examples\mcl_io.dll_Examples\VC++ (MFC)\ZtModular\ZtModular\Debug\BAT00001333402288.bat" with contents
[
@echo Manifest resource last updated at %TIME% on %DATE% > ".\Debug\mt.dep"
]
Creating command line """d:\soft\Project Examples\MCL_ZT_Modular_Examples\mcl_io.dll_Examples\VC++ (MFC)\ZtModular\ZtModular\Debug\BAT00001333402288.bat"""
Output Window
  
Compiling...
ZtModularDlg.cpp
d:\soft\project examples\mcl_zt_modular_examples\mcl_io.dll_examples\vc++ (mfc)\ztmodular\ztmodular\ztmodulardlg.cpp(187) : warning C4996: 'wcscpy' was declared deprecated
        c:\program files\microsoft visual studio 8\vc\include\string.h(250) : see declaration of 'wcscpy'
        Message: 'This function or variable may be unsafe. Consider using wcscpy_s instead. To disable deprecation, use _CRT_SECURE_NO_DEPRECATE. See online help for details.'
Linking...
Embedding manifest...
Results
  
Build log was saved at "file://d:\soft\Project Examples\MCL_ZT_Modular_Examples\mcl_io.dll_Examples\VC++ (MFC)\ZtModular\ZtModular\Debug\BuildLog.htm"
ZtModular - 0 error(s), 1 warning(s)