Found 200 matches (page 1 of 20)
representative and distributor. Suppliers are nominated for awards in various categories by SPDEI member Gandolfini nominated Mini-Circuits as a candidate among several suppliers in the RF category based on 30
a �2-dB level of nominal LO power requirements. This is useful for system designers when budgeting
3300 MHz and local-oscillator (LO) signals from 2300 to 7400 MHz and a nominal LO level of +13 dBm to
frequencies, two nominally equal-amplitude output signals are produced at the sum and the difference of
drive level. Remember that as LO level increases over the nominal (to +10 dBm for a level 7 mixer), also indicates the susceptibility of the mixer to unwanted signals. Q. I need a mixer that nominally
with LO input as low as -6 dBm. Examples, with their nominal LO levels, are: MACA-242H+ (-3 dBm, can be taken nominally as the inverse of the derating: (150 - 25) / 0.3W = 417°C per watt. Maximum
nominal level of +17 dBm to produce RF output signals from 2600 to 7100 MHz (well in excess of the
will meet the system requirements. The LO level is defined by the nominal LO power available to level can have a range of about ± 3 dB about this nominal level. Linearity performance is tightly
resistor should have a nominal value of 100 and 150 ohms for TCP-2-10 and TCP-2-10-75 respectively. Each capacitor should be of NPO type with a nominal value of 1.5pF. For TCP-2-10 use both C1 and C2 as
ground reference, after subtracting the 180-degree nominal value of the phase-split. Measurement Method: are typically the “1% values”. Their nominal values, having increments of 2%, could thus differ from