Found 200 matches (page 10 of 20)
demodulator. The quadrature signals aregenerated by the 90-deg. hybrid. The I/Q signal's magnitude and into two equal-amplitude signals which are 90 deg. apart, and the RF signal is split into two rejection/suppression (Fig.4), the low-frequency generator output is split into two signals at 0 respectively. An alternate technique is to use two generators to obtain equal amplitude signals that are 90 A bipolar pulse signal is applied at data ports to produce an RF output signal phase-modulated by 0
determines the power rating of the power splitter/combiner. If two signals at different RF frequencies, are being added; then each signal will appear at the S port with a 3 dB loss. The internal resistor absorbs the 3 dB power loss for each signal. Note: If the two signals were equal in phase, and the isolation measurement. Assume a 0 dBm input from the RF generator at port A. First, the signal ports can result in reflected signals that could exceed the power limits of the internal terminations.
the frequency of the control signals. For the DAT and ZX76 models, the switching control frequency Generator operation. Please note that models with dual supply voltages do not have this issue and signals the customer can use a Pull-up or Pull-down scheme using resistor values from 0Ω to 100kΩ. ZX76 attenuators? The single supply models (-SP, -PP suffix) have an internal generator producing level of the generator is typically lower than -120dBm, noise level of dual supply models (-PN, - SN
generators and want to maintain a 50-ohm load on the generator that is not switched to the common port, switching speed The most popular parameters are listed below: TRise = Rise Time, time for RF signal to rise from 10% to 90% of the "on" level. TFall = Fall Time, time for RF signal to fall from 90% two outputs, can I use the switch in the opposite direction? I want to connect signals to the polarity of the RF signal, so that the diode appears as a fixed impedance (low impedance for positive
±.005"HM BRACKET OPTION ONE SET OF 2 EACH. N K P R SYNTHESIZED SIGNAL GENERATOR
LV1754 F N K P G J A B C D 2x Diam. L ±.005"HM E SYNTHESIZED SIGNAL GENERATOR N-TYPE FEMALE BRACKET
SIGNAL GENERATOR
USB / Ethernet Synthesized Signal Generator FX-30G-RC Typical Performance Curves Test Conditions: @ Temperature = +25°C. -2.00 -1.60 -1.20 -0.80 -0.40 0.00 0.40 0.80 1.20 1.60 2.00 0 3000 6000 9000 12000 15000 18000 21000 24000 27000 30000 Po w er A cc ur ac y [d B] Frequency [MHz] Power deviation Synthesized Signal Generator FX-30G-RC Typical Performance Curves Test Conditions: @ Temperature = GHz 17.8 GHz 21.2 GHz 25.2 GHz 28 GHz 30 GHz Page 2 of 3 USB / Ethernet Synthesized Signal Generator
USB Synthesized Signal Generator -45 -40 -30 -20 -10 0 10 14 17 20 dBm dBm dBm dBm dBm dBm dBm dBm dBm dBm 10 0.143 0.186 0.079 0.133 0.920 0.929 0.789 0.609 0.392 0.009 50 0.200 0.253 0.157 0.139 0.326 0.328 0.271 0.165 0.033 -0.223 100 0.055 0.104 0.056 0.032 0.180 0.188 0.107 0.015 -0.093 -0.325 (dBm)Frequency (MHz) REV. OR FX-30G-RC 220316 Page 1 of 3 USB Synthesized Signal Generator FX-30G-RC Typical 220316 Page 2 of 3 USB Synthesized Signal Generator F2 F3 F0.5 F1.5 F2.5 F2 F3 F0.5 F1.5 F2.5 10
REV. OR SSG-15G-RC 190416 Page 1 of 2 USB Synthesized Signal Generator SSG-15G-RC Typical Performance Data -2.5 -2.0 -1.5 -1.0 -0.5 0.0 0.5 1.0 1.5 2.0 2.5 -50 -45 -40 -35 -30 -25 -20 -15 -10 -5 0 5 10 15 Po w er A cc ur ac y (d B) Power (dBm) Power Deviation from Nominal Vs. Output Power 10 MHz 200 MHz 500 MHz 1000 MHz 2000 MHz 3000 MHz 5000 MHz 8000 MHz 10000 MHz 12000 MHz 15000 MHz 3 5 7 9 11 SSG-15G-RC 190416 Page 2 of 2 USB Synthesized Signal Generator SSG-15G-RC Typical Performance Data