Found 200 matches (page 2 of 20)
should have a nominal value of 75 or 50 ohms for TCD-13-4-75 and TCD-13-4 respectively. Actual data
a nominal return loss of 10 to 12 dBr. The phase variation exceeds 3600 within specified operating
These three-port devices feature a nominal return loss of 10 to 12dB, with electronically adjustable
Status is nominal 0x1 Unspecified Error. RF output OFF (blocking); Reset controller. 0x2 High
75˚C for air-cooled systems The amount of reflected RF power: 25% of the nominal power rating of the PA (in mode 0) 125% of the nominal power rating of the PA (in mode 1) Note: See section 3.3 for more details. The total dissipated power: High limit: Nominal PA output power * 2 Shutdown limit: Nominal PA output power * 2.2 AN-50-003 Rev.: OR DCO-000695 (11/01/21) File: AN-50-003.docx This preferred. A conservative setting would be the nominal value of the PA’s output power + 33%. This mode
ground terminal for use with an external remote shutoff circuit. The nominal RF power output of 25 watts
a nominal gain of 11 dB. Figure 1 is a photograph of the amplifier. Figure 2 shows how the power supply. It operates in Class-A and produces a nominal output power of 1 watt. Figure 1 – HELA-10
Darlington amplifiers. Table 1 Device Voltage Variation with Current and Temperature Model No. Nominal user might need to consider: • Available nominal values, tolerance and temperature coefficient of the available are generally the “1% values”. The nominal values, having increments of 2%, could thus differ from ±1%. As an example, consider the ERA-51SM+ being used with a 9-volt supply. Since the nominal device 2.3% + 0.5% = 2.8% error in current, which is 1.8 mA for a nominal value of 65 mA. Besides, the
the entire back surface of the boards. Copper thickness on each side is nominally 2 mils, due to
time). The worst case is when the current source jumps from zero to the nominal current value conduct not only the current source pumps in the nominal current Icc=17mA, but the charged output resistor is less than from the ideal current source at nominal current. The drawback is weaker RF operate at nominal current of 17 mA. Keithley 236 power supply was used as a current source and current step of 14 mA (less than nominal 17 mA) is applied, the peak voltage reaches the value of