Found 200 matches (page 3 of 20)
Deviation of a distribution. All nominally identical things differ one from another to a greater or
ZHL-2425-250X+ can generate and dissipate a significant amount of power. At the nominal operating
nominally specified at 50 ohms (and, in the case of cable-television or CATV systems, 75 ohms), their
tolerances in the broad DC to 18GHz band, and each family contains 15 models with nominal attenuation from
these are not ideal components and, in addition to the tolerance on their nominal attenuation values,
Operation of Microwave Precision Fixed Attenuator Dice up to 40 GHz (AN-70-019) I. INTRODUCTION Mini-Circuits’ YAT-D-series MMIC attenuator dice (RoHS compliant) are fixed value, absorptive attenuators fabricated using highly repetitive MMIC processing with thin film resistors on silicon substrates. They contain through-wafer Cu metallization vias to realize low thermal resistance and very wideband operation. YAT attenuator dice are available from stock with nominal attenuation values of 0 to
nominal step size / resolution and the pin-diode characteristic means the max attenuation achievable dB typ Attenuation Range 0-25 dB guaranteed 0-40 dB nominal (frequency dependent) 0-30 dB Attenuation are the attenuation characteristic at max attenuation and the nominal step size (0.25 dB, compared
nominal attenuation spec? A. The nominal or average value of attenuation of a particular attenuator is guaranteed to be within the nominal spec window, and is measured at the low frequency end of the
tolerance The allowable unit-to-unit variation in nominal coupling. coupling flatness The maximum
designed with 24dB return loss, the sum will be within 0.6dB of nominal. Q. What makes Mini-Circuits'